Custom Modulation

Custom IQ - ASK & PSK & QAM

The Custom IQ Type: ASK & PSK & QAM waveform setup allows you to configure a frame with multiple data segments and/or idle segments. For each data segment, the modulation type can be further configured using a graphical constellation settings editor.

Quick Setups

Modulation Config

Save to 89600 VSA Setup

Custom IQ Selection

Custom IQ Type

Custom ASK & PSK & QAM

Symbol Rate

Filter

Filter

Alpha

Bandwidth

BT

Length(symbol)

Filter Coefficient

Segments

Add Segment

Remove Segment

Name

Type

Constellation

Number of Symbols

Ramp Samples

Bits Per Symbol

Differential

Offset

Shift

Rotation

Payload Data

Pattern Bits

User File

PN Seed(Hex)

Offset

Quick Setups

Use this drop-down menu to select a modulation type from several supported formats. A single data segment using that modulation type appears in the segment list below. Click the cell in the Constellation column to open the Constellation Setting window, providing a graphical display and editing features. Quick setups enable you to configure complex signals for signal generation, equivalent to 89600B VSA setups in signal analysis.

DVB-S2 and DVB-S2X quick setups also add a PLHEADER segment before the data segment, as defined in the standard.

Quick Setups IQ Settings

Standard

Modulation

Symbol Rate

Filter

DVB-S2

QPSK

 

1.0 Msps

RNYQ (0.5)

8PSK

 

16APSK

4+12APSK 2/3, 4+12APSK 3/4, 4+12APSK 4/5, 4+12APSK 5/6, 4+12APSK 8/9, 4+12APSK 9/10

32APSK

4+12+16APSK 3/4, 4+12+16APSK 4/5, 4+12+16APSK 5/6, 4+12+16APSK 8/9, 4+12+16APSK 9/10

DVB-S2X

QPSK

 

1.0 Msps

RNYQ (0.5)

8PSK

 

8APSK

2+4+2APSK 100/180, 2+4+2APSK 104/180

16APSK

4+12APSK Normal 26/45; 4+12APSK Normal 3/5; 4+12APSK Normal 28/45; 4+12APSK Normal 23/36; 4+12APSK Normal 25/36; 4+12APSK Normal 13/18; 4+12APSK Normal 140/180; 4+12APSK Normal 154/180; 4+12APSK Short 7/15; 4+12APSK Short 8/15; 4+12APSK Short 26/45; 4+12APSK Short 3/5; 4+12APSK Short 32/45; 8+8APSK Normal 90/180, 96/180, 100/180; 8+8APSK Normal 18/30; 8+8APSK Normal 20/30

32APSK

4+12+16APSK Normal 2/3, 4+12+16APSK Short 2/3, 4+12+16APSK Short 32/45, 4+8+4+16APSK 128/180, 4+8+4+16APSK 132/180, 4+8+4+16APSK 140/180

64APSK

16+16+16+16APSK 128/180, 8+16+20+20APSK 7/9, 8+16+20+20APSK 4/5, 8+16+20+20APSK 5/6, 4+12+20+28APSK 132/180,

128APSK

128APSK 135/180, 128APSK 140/180

256APSK

256APSK 116/180, 256APSK 124/180, 256APSK 128/180, 256APSK 135/180, 256APSK 20/30, 256APSK 22/30

APCO25

C4FM

4FSK (0.6 kHz, 1.8 kHz, -0.6 kHz, -1.8 kHz)

4.8 ksps

NYQ (0.2) + 1/Sinc

CQPSK*

Pi/4 DQPSK

4.8 ksps

NYQ

HCPM

4FSK (1 kHz, 3 kHz, -1 kHz, -3 kHz)

6 ksps

APCO25 HCPM

HDQPSK

Pi/4 DQPSK

6 ksps

APCO25 HDQPSK

TETRA

Pi/4 DQPSK

18 ksps

RNYQ (0.35)

NXDN

4800 bps

4FSK (0.35 kHz, 1.05 kHz, -0.35 kHz, -1.05 kHz)

2.4 ksps

RNYQ (0.2) + Sinc

9600 bps

4FSK (0.8 kHz, 2.4 kHz, -0.8 kHz, 2.4 kHz)

4.8 ksps

RNYQ (0.2) + Sinc

dPMR

4FSK (0.35 kHz, 1.05 kHz, -0.35 kHz, -1.05 kHz)

2.4 ksps

RNYQ (0.2)

DECT

2FSK (-288 kHz, 288 kHz)

1.152 Msps

Gaussian (0.5)

DMR

4FSK (0.648 kHz, 1.944 kHz, -0.648 kHz, -1.944 kHz)

4.8 ksps

RNYQ (0.2)

ARIB

T98/T61*

Pi/4 DQPSK

9.6 ksps

RNYQ (0.2)

T102

4FSK (0.33 kHz, 0.99 kHz, -0.33 kHz, -0.99 kHz)

4.8 ksps

ARIB T102 RNYQ (0.2) + Gaussian (0.769)

Zigbee

BPSK

BPSK

600 ksps

NYQ (1)

OQPSK

OQPSK

1 Msps

Half Sine

WiSUN (802.15.4g)

2FSK 50/1

2FSK (-25 kHz, 25 kHz)

50 ksps

Gaussian (0.5)

2FSK 100/0.5

2FSK (-25 kHz, 25 kHz)

100 ksps

Gaussian (0.5)

ITU-T G.9959

R2

2FSK (-20 kHz, 20 kHz)

40 ksps

Rectangle

R3

2FSK (-29 kHz, 29 kHz)

100 ksps

Gaussian (0.6)

802.15.3d

CES: pi/2 BPSK

Frame Header: pi/2 BPSK

Payload: 64QAM

25.92 Gsps

RNYQ (0.25)

* For APCO25 CQPSK and ARIB T98/T61, the ALC is set to off to achieve better EVM. For all other cases, the ALC is on.

Payload, Idle Interval, Ramp Symbols, and Number of Symbols will be set to default values.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:SETup C4FM|HCPM|TETRa|DECT|HDQPsk|ZIGBEE_BPSK|ZIGBEE_O_QPSK|DMR|ARIB_T98| ARIB_T61|ARIB_T102|WI_SUN_2FSK_50_1|WI_SUN_2FSK_100_0P5|ITU_T_G9959_R2|ITU_T_G9959_R3| CQPSk| NXDN_4800BPS| NXDN_9600BPS| DPMR|DVB_S2X_256APSK_116_180| DVB_S2X_256APSK_124_180| DVB_S2X_256APSK_135_180| DVB_S2X_256APSK_20_30| DVB_S2X_256APSK_22_30| DVB_S2X_128APSK_135_180| DVB_S2X_128APSK_140_180| DVB_S2X_16_16_16_16APSK_128_180| DVB_S2X_8_16_20_20APSK_7_9| DVB_S2X_8_16_20_20APSK_4_5| DVB_S2X_8_16_20_20APSK_5_6| DVB_S2X_4_12_20_28APSK_132_180| DVB_S2X_4_12_16APSK_NORMAL_2_3| DVB_S2X_4_12_16APSK_SHORT_2_3| DVB_S2X_4_12_16APSK_SHORT_32_45| DVB_S2X_4_8_4_16APSK_128_180| DVB_S2X_4_8_4_16APSK_132_180| DVB_S2X_4_8_4_16APSK_140_180| DVB_S2X_4_12APSK_NORMAL_26_45| DVB_S2X_4_12APSK_NORMAL_3_5| DVB_S2X_4_12APSK_NORMAL_28_45| DVB_S2X_4_12APSK_NORMAL_23_36| DVB_S2X_4_12APSK_NORMAL_25_36| DVB_S2X_4_12APSK_NORMAL_13_18| DVB_S2X_4_12APSK_NORMAL_140_180| DVB_S2X_4_12APSK_NORMAL_154_180| DVB_S2X_4_12APSK_SHORT_7_15| DVB_S2X_4_12APSK_SHORT_8_15| DVB_S2X_4_12APSK_SHORT_26_45| DVB_S2X_4_12APSK_SHORT_3_5| DVB_S2X_4_12APSK_SHORT_32_45| DVB_S2X_8_8APSK_NORMAL_90_180_96_180_100_180| DVB_S2X_8_8APSK_NORMAL_18_30| DVB_S2X_8_8APSK_NORMAL_20_30| DVB_S2X_2_4_2APSK_100_180| DVB_S2X_2_4_2APSK_104_180| DVB_S2X_SCRAMBLED_2_4_2APSK_100_180| DVB_S2X_SCRAMBLED_2_4_2APSK_104_180| DVB_S2X_SCRAMBLED_256APSK_20_30| DVB_S2X_SCRAMBLED_256APSK_22_30| DVB_S2X_QPSK| DVB_S2X_8PSK | DVB_S2_QPSK| DVB_S2_8PSK| DVB_S2_4_12APSK_2_3| DVB_S2_4_12APSK_3_4| DVB_S2_4_12APSK_4_5| DVB_S2_4_12APSK_5_6| DVB_S2_4_12APSK_8_9| DVB_S2_4_12APSK_9_10| DVB_S2_4_12_16APSK_3_4|DVB_S2_4_12_16APSK_4_5 | DVB_S2_4_12_16APSK_5_6 | DVB_S2_4_12_16APSK_8_9| DVB_S2_4_12_16APSK_9_10| _802_15_3D

 

SCPI Example

 

Couplings

 

Preset

 

State Saved

No

Modulation Config

The Modulation Config option is available only when you set the Custom IQ Type to QAM & ASK & PSK.

You need to set the following three parameters for Modulation Config:

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:CONFig:MODulation "SymbolRate: <real>, NumberOfSymbols: <integer>, ModulationType: OOK|ASK2|ASK4|ASK8|BPSK|QPSK|PSK8|QAM16|QAM32|QAM64|QAM128|QAM256|QAM512|QAM1028|QAM2048|QAM4096"

SCPI Example

RAD:CMOD:WAV:IQ:QAPS:CONF:MOD "SymbolRate: 1000000, NumberOfSymbols: 1000, ModulationType: QAM16"

Couplings

 

Preset

 

State Saved

Yes

 

Save to 89600 VSA Setup

This feature saves the Custom IQ configuration as an 89600B VSA setup file, making it easier to configure complex constellations, such as 256APSK.

VSA software must be version 18.0 or later to support Custom IQ demodulation. If there is more than one data segment configured in the list, they will be saved as VSA setup file with FlexFrame measurement, which was supported from VSA2022 release. Idle segments cannot be saved to the setup file.

ASK & PSK & QAM

Differential and offset modulation types (e.g. pi/4 DQPSK or OQPSK) are found under DigitalDemod on the VSA.

The VSA does not support the APCO25 HDQPSK filter.

FSK

FSK configurations are found under DigitalDemod on the VSA.

The VSA does not support ARIB T102 and NXDN filters.

For added convenience, you can save the VSA setup as a quick setup in the VSA's Custom IQ Demod Property window. To do this, recall the PathWave Signal Generation VSA setup file, perform the measurement, and then click Save As Quick Setup. Now, whenever you click Quick Setups, you will find your previously saved setup listed among the other setups provided with the VSA software. Using this method, you no longer need to recall the PathWave Signal Generation VSA setup file each time you want to perform a measurement.

Custom IQ Selection

Custom IQ Type

Select the type of Custom IQ.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:TYPE QAPSk|FSK|SOQPsk|ARTM

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:TYPE?

SCPI Example

 

Couplings

 

Preset

QAPSk

State Saved

Yes

Custom ASK & PSK & QAM

Symbol Rate

Sets the symbol rate of the waveform.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SRATe <real>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SRATe?

SCPI Example

 

Couplings

 

Preset

1000000

State Saved

Yes

Minimum Value

1000

Maximum Value

100000000000

Filter

Filter

Choices: Low Pass| Gaussian | Root Nyquist | Nyquist | Rectangle | APCO25 HDQPSK | Half Sine | User Defined

Default: Root Nyquist

Select the filter type to be applied to the waveform.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:FILTer:TYPE RNYQuist|NYQuist|GAUSsian|LPASs||RECTangle|UDEFined||AHDQpsk|HSINe|

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:FILTer:TYPE?

SCPI Example

 

Couplings

 

Preset

RNYQuist

State Saved

Yes

Alpha

Sets the alpha factor of the Root Raised Cosine, Root Nyquist, or Nyquist filter.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:FILTer:ALPHa <real>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:FILTer:ALPHa?

SCPI Example

 

Couplings

 

Preset

0.5

State Saved

Yes

Minimum Value

0.01

Maximum Value

1

Bandwidth

Sets the bandwidth for a low-pass filter.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:FILTer:BWIDth <real>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:FILTer:BWIDth?

SCPI Example

 

Couplings

 

Preset

1000000

State Saved

Yes

Minimum Value

1000

Maximum Value

1000000000

BT

Sets the BT product of the Gaussian filter. It is visible when Filter Type is set to Gaussian.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:FILTer:BT <real>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:FILTer:BT?

SCPI Example

 

Couplings

 

Preset

0.5

State Saved

Yes

Minimum Value

0.1

Maximum Value

1

Length(symbol)

Sets the length of the filter in symbols.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:FILTer:SYMBol:LENGth <integer>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:FILTer:SYMBol:LENGth?

SCPI Example

 

Couplings

 

Preset

32

State Saved

Yes

Minimum Value

1

Maximum Value

2048

Filter Coefficient

Opens a ClosedFilter Editor window where you can import, export, and edit filter coefficients. A convenient plot of the filter's impulse response is displayed and updates as coefficients are changed. Imported and exported coefficient files are in text (*.txt) or comma-separated values (*.csv) format.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:FILTer:COEFficient <string>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:FILTer:COEFficient?

SCPI Example

:RADio:CMODulation:WAVeform:IQ:QAPSk:FILTer:COEFficient "0,1,2"

Couplings

Filter coefficients are separated by "," for example 0,0,1,0,2

Preset

"1"

State Saved

Yes

Segments

Add Segment

Choices: Data Segment | Idle Segment

Use the plus icon (+) in the GUI to add a segment to the end of the segments column. Choose between data and idle segments.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent:ADD DATA|IDLE

SCPI Example

 

Couplings

The maximum count of segments is 1024. If the current count is 1024 and you try to add a new segment, the error -224 "Illegal parameter value; Failed to add segment because limit of 1024 has been reached" will be shown.

Preset

 

State Saved

No

Remove Segment

Use the minus icon (-) in the GUI to remove the selected segment from the segments column.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent:DELete <integer>

SCPI Example

 

Couplings

If index to be deleted is less than 0 or greater than the current count – 1, the error -224 "Illegal parameter value; Failed to delete segment because invalid segment index" will be shown.

Preset

 

State Saved

No

Name

Sets the name of the segment. Click on the name to edit.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:NAME <string>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:NAME?

SCPI Example

 

Couplings

 

Preset

"DataSeg"

State Saved

Yes

Type

Displays the segment type: DATA or IDLE.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:TYPE?

SCPI Example

 

Couplings

 

Preset

DATA

State Saved

Yes

Constellation

Choices: BPSK | QPSK | 8PSK | 16QAM | 32QAM | 64QAM | 128QAM | 256QAM | 512QAM | 1024QAM | 2048QAM | 4096QAM | User defined

Default: 16QAM

Displays the modulation type for the segment. Click the arrow to open the Constellation Setting window where you can customize the constellation.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:CONStellation:NAME <string>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:CONStellation:NAME?

SCPI Example

 

Couplings

 

Preset

"16QAM"

State Saved

Yes

Number of Symbols

Set the length of the segment in number of modulated symbols.

It is better to set an even number for Pi/4 DQPSK and Pi/8 D8PSK case for non-burst signals.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:SYMBols:COUNt <integer>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:SYMBols:COUNt?

SCPI Example

 

Couplings

 

Preset

1000

State Saved

Yes

Minimum Value

1

Maximum Value

8388608

Ramp Samples

Set the length of ramp samples for each data segment. Not configurable for idle segments.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:RAMP:SAMPles <integer>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:RAMP:SAMPles?

SCPI Example

 

Couplings

 

Preset

0

State Saved

Yes

Minimum Value

0

Maximum Value

1000

Bits Per Symbol

Displays the number of bits contained in one modulated symbol.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:BPSYmbol?

SCPI Example

 

Couplings

 

Preset

4

State Saved

Yes

Differential

Enable or disable the differential encoding for the segment. This can be enabled only for BPSK, QPSK, and 8PSK constellations. Differential and Offset modes cannot be enabled simultaneously.

The last symbol of the waveform may be modified to ensure that the demodulated bits are correct in the beginning of the waveform.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:DIFFerential ON|OFF|1|0

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:DIFFerential?

SCPI Example

 

Couplings

 

Preset

OFF

State Saved

Yes

Offset

Enable or disable IQ offset by half symbol time. This can only be enabled for a QPSK constellation. Differential and Offset modes cannot be enabled simultaneously.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:OFFSet ON|OFF|1|0

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:OFFSet?

SCPI Example

 

Couplings

 

Preset

OFF

State Saved

Yes

Shift

Enable or disable shift for phase rotation. When enabled, the phase rotation is only applied to the odd symbol. For example: pi/2 shift BPSK, pi/4 shift QPSK. When shift is enabled, differential and offset are disabled and set to false. When differential or offset is enabled, shift is disabled and set to false.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:SHIFt ON|OFF|1|0

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:SHIFt?

SCPI Example

 

Couplings

 

Preset

OFF

State Saved

Yes

Rotation

Set an additional phase rotation applied to the constellation for the segment. To view the phase rotation, you can check the Show Rotation checkbox in the Constellation Setting window.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:ROTation <real>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:ROTation?

SCPI Example

 

Couplings

 

Preset

0

State Saved

Yes

Minimum Value

0

Maximum Value

360

Payload Data

Choices: PN9 | PN15 | PN23 | Custom | User File

Default: PN9

Opens the ClosedData Setup editor to configure payload bits. You can also load, save, and create Closedcustom bit patterns.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:DATA:TYPE PN9|PN15|PN23|CUSTom|FILE

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:DATA:TYPE?

SCPI Example

 

Couplings

 

Preset

PN9

State Saved

Yes

Pattern Bits

Create custom bit patterns when the Payload Data type is set to Custom.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:DATA <string>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:DATA?

SCPI Example

 

Couplings

 

Preset

 

State Saved

Yes

User File

Set the Payload data file name when the Payload Data type is set to User File.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:DATA:FILE <string>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:DATA:FILE?

SCPI Example

 

Couplings

If you specify just the file name or relative path + file name, then it will be converted to absolute path + file name.

Examples:

  • For just the file name: custom.txt, it will be converted to <Documents>\Keysight\PathWave\SignalGenerator\Apps\custom.txt.

  • For relative path + file name: payload\custom.txt, it will be converted to <Documents>\Keysight\PathWave\SignalGenerator\Apps\payload\custom.txt.

If you specify the absolute path + file name, for example, C:\temp\test.txt, on the instrument, then error +671,"Application error;Invalid file path c:\temp\test.rxt." will be generated.

Preset

""

State Saved

Yes

PN Seed(Hex)

Set the Payload PN Seed when the Payload Data type is set to PN9, PN15, or PN23.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:DATA:PNSeed <integer>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:DATA:PNSeed?

SCPI Example

 

Couplings

 

Preset

1FF

Min 0
Max 8388607

State Saved

Yes

Offset

Set the Payload offset. This setting is applicable to all Payload Data types.

SCPI Command

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:DATA:OFFSet <integer>

[:SOURce]:RADio:CMODulation:WAVeform[:ARB]:IQ:QAPSk:SEGMent<segment>:DATA:OFFSet?

SCPI Example

 

Couplings

 

Preset

0

Min 0
Max 2147483647

State Saved

Yes

Carrier - Custom IQ